{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What is the difference between the leak sensors AP9325 and AP9326?
Issue:
What is the difference between the leak sensors AP9325 and AP9326?

Product line:
All InRow Units

Environment:
Data Center Cooling

Cause:

Resolution:
There are 3 main differences:
  1. AP9325 is used for the 300mm Gen1 InRow RC , InRow SC, InRow RD, and Environment  & Monitoring Systems, whereas the AP9326 is just for the Gen1 600mm InRow RP, RD, and RC
  2. The AP9326 is the extension cable of AP9325.
  3. The connection for AP9325 is RJ45, whereas the AP9326 connection is a 2 prong Molex connector.  Please see below:
AP9326
600mm InRow CW600mm InRow DX
12
AP9325
3

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :