{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Smart-UPS VT-G3500; What is Generator Charge (GEN CHRG) mode feature, how does it work?
Issue:
What is Generator Charge (GEN CHRG) mode feature, how does it work?

Product line:
Smart-UPS VT – Galaxy 3500

Environment:
All Product models, All serial numbers

Cause:
Generator Charge is for de-rating the power the UPS uses for charging the battery when supplied from a generator.

Resolution:
The GEN CHRG (Generator Charge) mode can be activated via the display: Main Menu>System>Gen Chrg. The generator must supply a signal to the UPS to reduce charge.
UPS TB J106, Pins 7 & 8 are for external charge control. When 7 & 8 are closed, the UPS charges batteries with a pre-defined percentage (0-100%) of the maximum charging power. To be used in generator applications, or if special codes requires control of charging. See page 36 attached file, install guide.

Schneider Electric Algeria

Pièce(s) jointe(s)
Site Preparation and Installation Manual10-30KVA_990-1598B-EN.pdf [6.15 MB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :