{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Can your InRow Cooling Auto-Start after a Power Failure
Issue:
Can your InRow Cooling Auto-Start after a Power Failure

Product line:
InRow

Environment:
Data Center Cooling

Cause:

Resolution:
The InRow RC, RD, RP and SC will start automatically if the power is restored after a power failure. The unit will go to its last known state, ie if the unit was in standby, the unit would return to standby, or if the unit is on, the unit would return to the on state.

It is also possible to configure a Start up Delay of 0 to 999 seconds.

That can be done from:
  1. The Display: Configure Unit>General> Startup Delay
  2. The Network Management Card Interface: Unit>Unit Configuration> Startup Delay

Schneider Electric Algeria

En savoir plus
Produit :
Les articles qui pourraient être utiles
En savoir plus
Produit :