{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What input supply changes are necessary to feed a 208v Symmetra LX 240 VAC?
Symmetra LX can automatically adjust to input voltage between 200 and 240 volts. No change to the system is required to accommodate these voltages.  However, it is best practice to set the output voltage and frequency to match the input voltage and frequency.  This will help avoid problems with bypass operation of the UPS.  These changes can be made via the front display or the network management card.


Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :