Issue
Symmetra Power Array has a maximum redundancy alarm limit of N+2. The user cannot set this alarm to a value greater than 2. This means that if the user
Product Line
Symmetra Power Array
Environment
All serial ranges
Cause
The system is unable to support a value greater than 2 for the user configurable redundancy alarm.
Resolution
The system is not capable of this function.
Please Note: The Symmetra can report on current redundancy levels greater than N+2, such as via the PowerView Status menu or Network Management Card, etc. The system is simply not capable of alarming when the redundancy limit falls below N+3. This is not considered a typical use case anyway.
Publié pour:Schneider Electric Algeria