Issue
Matrix-UPS is not providing any output power to the receptacles on the rear of the UPS.
Product Line
Matrix-UPS
Environment
All
Cause
There is an ON/OFF circuit breaker switch located on the back plate of the Matrix-UPS IU (Isolation Unit, lower half of the Matrix-UPS) just above the NEMA L14-30 receptacle. This breaker controls the UPS output to the L14-30 receptacle (as well as the NEMA 5-15 receptacles on the Matrix-UPS 3000 model only). On the Matrix-UPS 5000, this switch controls the L14-30 receptacle only. If the Matrix-UPS is powered on and there is no output to the L14-30 receptacle (or any of the 5-15 receptacles on a Matrix-UPS 3000) check this switch to ensure that it is set to ON (to the right). This symptom is often experienced on a new installation.
Resolution
Close the breakers to restore power to the receptacles. If the breaker has tripped while the unit was in service, this was due to an overload to the circuit by loads downstream of the Matrix-UPS. Evaluate the circumstances and correct by reducing the number of connected devices.
Publié pour: Schneider Electric Algeria
Besoin d'aide ?
Commencez ici !
Trouvez des réponses dès à présent Rechercher une solution par vous-même ou contacter l'un de nos experts.
Contactez le support
Contactez notre équipe du service client pour obtenir plus d'informations, un support technique, une assistance en cas de plaintes, etc.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Parcourir la FAQ
Obtenez les réponses dont vous avez besoin en parcourant la foire aux questions (FAQ) par sujet.
Contacter le service commercial
Effectuez une demande de renseignements en ligne et un expert vous contactera.