Yes. There are no country or region specific versions of the SYMIM5. It is universal and can be used in both split-phase (208/240V) Symmetra LX models as well as 3:1 / 1:1 (220/230/240V or 380/400/415V) Symmetra LX models.
Publié pour:Schneider Electric Algeria