{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Electrolyte Levels of All Single-phase Symmetra Battery Systems

Issue

What are the electrolyte levels of single phase Symmetra UPS and battery systems?


Product Line

Symmetra Power Array
Symmetra RM
Symmetra LX


Environment

All serial ranges


Cause

This document contains the electrolyte levels found in the battery modules used by each single phase Symmetra system.  This information can sometimes be needed for regulatory compliance in certain jurisdictions.


Resolution

Symmetra Power Array
SYBATT: Each SYBATT contains (10) 12V 7.2Ah batteries installed in series. The total amount of electrolyte in (1) SYBATT is 0.845 gallons.

Symmetra 12k RM
SYBT3: Each SYBT3 contains (10) 12V 7.2Ah batteries installed in series. The total amount of electrolyte in (1) SYBT3 is 0.845 gallons.

Symmetra 6k RM
SYBT2: Each SYBT2 contains (10) 12V 5.1 Ah batteries installed in series. The total amount of electrolyte in (1) SYBT2 is 0.55 gallons.

Symmetra LX
SYBT5: Each SYBT5 contains (10) 12V 9Ah batteries installed in series. The total amount of electrolyte in (1) SYBT5 is 0.95 gallons.




Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :