{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
How to replace a NetworkAIR FM Series Filter Replacement

Article available in these languages: Espagnol

Issue:
NetworkAIR FM Series Filter Replacement

Product line:
FM35-50

Environment:
All serial numbers

Cause:
Install, Maintenance

Resolution:
The spare part number for the filters is W0M-74350. The part number W0M-74530 ships as 1 box of 5 filters.  5 filters are required per unit.

The filtration of conditioned air is extremely vital to maintaining the clean, particle-free environment required by electrical equipment. The system uses 30% efficient (100 microns) (ASHRAE 52.1-92), 4” (102 mm) deep filters, with full depth filter pleats. Deeper filters produce a lower pressure drop, requiring less energy during normal operation. Filters are replaceable through the front of the upflow unit, and through the top of the downflow unit.

The technical specifications are as follows:

Net Weight 2.27 kg5lbs
Maximum Height102.00 mm4in
Maximum Width325.00 mm12.8in
Maximum Depth756.00 mm29.7in

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :