{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Halon and FM 200 Leakage and Detection
"NetBotz appliances with the use of third party 4-20mA sensors can be used for detecting leakage of FM-200/Halon.

The following third party sensor will work with the NetBotz 4-20mA pod. Newer NetBotz that do not work with this pod may also have a 4-20 input directly on the device itself.:

The SSG-MCD Suppression System Guard

This system detects Halon1301 and FM-200 fire suppression agents and optionally it can be built with 4-20mA output.

SSG-MCD User's Guide (see page 8)
"

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :