{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Disconnecting and Reconnecting a Configured RS232-Based Sensor or Output Control Device Can Cause Device Settings to be Lost
Issue:

Disconnecting and Reconnecting a Configured RS232-Based Sensor or Output Control Device Can Cause Device Settings to be Lost

Product Line:

NetBotz

Environment:

NetBotz 450, 455, 550, and 570.

RS232 sensor connections

Cause:

Settings associated with RS232-based sensors or output control devices may not be preserved if the device is disconnected and then reconnected.

Resolution:

Once you have connected and configured settings for an RS232-based sensor or device, do not disconnect or relocate this device unless you are prepared to reconfigure the device.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :