{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X
Issue:
Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X

Product Line:
NetBotz
Pelco Cameras

Environment:
NetBotz NBWL0455 and NBRK0570
4.X botzware
Pelco camera support

Cause:
Not all Pelco cameras have been tested with NetBotz 4.0 botzware.

Resolution:

Please note that the NetBotz 3xx and NetBotz NBRK0450/0451 do not support the Pelco integration.


The initially supported Pelco cameras from version 3.x firmware are:
Pelco Camera ModelProduct FamilyFirmware Version Tested
IP3701H-2IPUnavailable
IP110-CHV9IP110 Camclosure®Unavailable
SD4N-W0Spectra Mini IPUnavailable



The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.0. The Sarix line of Pelco cameras have been added to testing:
Pelco Camera ModelProduct FamilyFirmware Version Tested
IXS0CSarix IX1.7.19.9080-A1.5842
IXE20DNSarix Enhanced1.7.19.9081-A1.5843
IX30DNSarix IX1.7.8.9080-A1.5288
IMSOC10Sarix IME1.7.41.9260-O2.6725
SD4N-W0Spectra Mini IP 1.2.15


With the release of Botzware 4.2, the following list of additional Pelco cameras and firmwares have also been tested:
Pelco Camera ModelProduct FamilyFirmware Version Tested
IMSOC10Sarix1.8.2
IM10C10Sarix1.8.2
IX30DNSarix IX1.8.2
D5118Spectra HD1.8.2
TXB-NSpectra IV IP1.8.2
DD4N-W0Spectra Mini IP1.2.15
IP110IP110 Camclosure®1.0.47
IP3701IP1.0.10

The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.4:
Pelco Camera ModelProduct FamilyFirmware Version Tested
IM10C10Sarix1.9.2
IMS0C10Sarix1.9.2
D5118 Spectra HD1.9.2
IME119Sarix Enhanced2.1.2.0.8280-A0.0

The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.5.3:
Pelco Camera ModelProduct FamilyFirmware Version Tested
IL 10SarixUnavailable

The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.6.3:
Pelco Camera ModelProduct FamilyFirmware Version Tested
IJP121-1ISSarix1.16.37

Important Note:

Pelco Sarix Pro models that were originally listed as supported do not correctly update the resolution settings presented to NetBotz appliances. NetBotz can no longer support Sarix Pro models due to this limitation of the Pelco camera and they have been removed from this compatibility matrix.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :