{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Will the NetShelter SX leveling feet support the full weight of the cabinet and its contents?
Issue:
Can the full weight of the NetShelter cabinet rest on the leveling feet?
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Cabinets are leveled using the leveling feet so  they need to bear the full weight of the cabinet and it's contents. (static load rating)
Resolution:
Yes, the leveling feet can support the cabinet up to the rated static load rating of the cabinet.
FAQ FA158656 also contains information regarding shipping load, dynamic load and static load ratings.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :