{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What is the AR8395 Busbar Amp rating?
Issue:
What is the Amp rating for the AR8395 busbar?

Product Line:
NetShelter Accessories

Environment:
AR8395

Cause:
Equipment in the NetShelter must be grounded.

Resolution:
See attached document, or explanation below.

AR8395 Busbar Amp Rating

As of this writing (April 2012)  the AR8395 busbar has not been rated for power grounding. It is designed for low voltage applications. Its intended use is to ground equipment chassis of switches, routers, AV and other low voltage IT equipment to reduce noise from the system. Because of this intended use the AR8395 Busbar has not been rated for amperage. Should this product be rated in the future this document will be updated.

Schneider Electric Algeria

Pièce(s) jointe(s)
AR8395 Buss Bar Amp Rating.pdf [4.54 KB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :