{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Configuration of an APC USB UPS and Multiple USB Devices

Article available in these languages: Espagnol

Issue:

What does APC recommend for configuring an APC USB UPS and Multiple USB Devices?


Product Line:

Back-UPS and Back-UPS PRO


Environment:

N/A


Cause:

N/A


Resolution:

Peripherals: If you are using a ""self-powered"" USB hub* to connect your USB peripherals to your PC, APC recommends plugging that hub into the Battery Backup outlets. Otherwise, when there is a loss of power, the hub and its connected peripherals will no longer function. This will inhibit the system shutdown initiated by the UPS or the user.

*A ""self-powered"" hub is defined as a hub that gets its power from the wall outlet as opposed to getting its power directly from the PC's USB port.

APC USB Compatible UPS: APC recommends when using any kind of external USB hub, that the UPS USB cable be plugged directly into a USB port located on the PC itself ( also known as the root hub). This will ensure communication will not be lost.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :