{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Using a UPS with X-10 Equipment

Article available in these languages: Thaï

Issue:

X-10 technology is a home control system that sends high frequency electrical signals that ""piggy-back"" the AC line to control common household items such as lights and appliances.

Product Line:

SurgeArrest, Back-UPS and Back-UPS PRO

Environment:

N/A

Cause:

APC devices are designed to filter out EMI (Electro Magnetic Interference) and RFI ( Radio Frequency Interference), which the X-10 technology appears to be when applied to the device.

Resolution:

The use of such technology does not adversely affect APC UPSs. However, a UPS or surge suppressor may absorb or filter out X-10 signals as UPSs and suppressors treat these signals as noise. The result, then, is that some X-10 equipment may cease to receive signals.

A possible solution is to install an X-10 isolator which prevents a UPS from filtering out these signals. One commercial solution is currently available from www.SmartHome.com. It is called a "noisy device filter".

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :