{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
APC AV rack mounting rails are too long for my enclosure.

Issue:

The rails supplied with my APC AV device are too long for my AV rack enclosure.


Product Line:

APC AV S-type Power Conditioners w/ Battery Back-UP

  • S10, S10BLK
  • S15, S15BLK
  • S20
  • RLC1080BLK
APC AV J-type Power Conditioners w/ Battery Back-UP
  • J10, J10BLK
  • J15, J15BLK


Environment:

All of the previously listed products.


Cause:

These units were initially shipped with a rail kit designed for standard IT racks. This was found to be inadequate for many AV specific racks.


Resolution:

APC has developed the SRAILKIT for mounting the APC S Type AV Power Conditioner with Battery, into any four post racks with depths ranging from 20"" to 28"". The kit includes an Installation guide, Mounting Hardware, Rack Mounting brackets and Screws.



Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :