{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Minimum and Maximum voltages missing in PowerChute Data Log when connected via USB enabled Smart-UPS or Microlink language Smart-UPS
Issue:
Minimum and Maximum voltages missing in PowerChute Data Log when connected via USB enabled Smart-UPS or Microlink language Smart-UPS

Product Line:
PowerChute Business Edition
PowerChute Serial Shutdown

Environment:
All supported OS

Cause:
The minimum and maximum voltage readings (Vmin/Vmax) do not get transmitted from the UPS when connected with the Smart-UPS via USB cable. These values are filled in when the same UPS is connected via the serial communications cable. This is a limitation of USB communications on a Smart-UPS. The current voltage at the time the data is being recorded does populate with the correct information.


Solution:
None at this time

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :