{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Video: How do I reset the super administrator password on my Digital IP KVM (KVM1116P, KVM1116R, KVM2116P, or KVM2132P only)?

Issue

The super administrator's password has been forgotten


Product Line
  • Rac Accessories - KVM Switches
    • KVM1116P / KVM1116R
    • KVM2116P
    • KVM2132P


Environment

All firmware revisions, all serial numbers


Cause

The password is unknown


Resolution

Perform the following password reset procedure:
  1. Turn off the power to the KVM Switch. Open the top cover of  KVM Switch, and short the jumper marked "Restore Default Password". Depending on the model, the jumper may be labeled differently. See the chart below.


KVM ModelJumper Number and Label on KVM Motherboard
KVM1116P / KVM1116RJ8 - Restore Password
KVM2116PJ25 - Restore Password
KVM2132PJ25 - Restore Password


(Rear of KVM2132P is shown at the top of the picture)
KVM motherboard
(Front of KVM2132P is shown at the bottom of the picture)
  1. With the jumper shorted, turn on power to the KVM Switch, and wait for the front panel LEDs of the KVM to flash in unison. When they start to flash, the reset is completed.
  1. Return the jumper to the open position, remove power from the KVM switch, and replace the cover.
  1. Turn the power back on for the device.



The assigned usernames and passwords will all be cleared. Start the OSD with the default username/password, which is apc/apc for KVM1116P, KVM2116P, and KVM2132P.

For a video tutorial on this procedure, please see below:


Note: Some KVM1116R's may have their jumper labelled as "Default Password":

Default password jumper location

Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :