{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
INTERNAL: MF-63103, MF-63123 to M400, or M800 Wiring Instructions (Airflow)

Article available in these languages: Russe




INTERNAL
Issue:
How to wire an actuator for an Airflow unit.

Product Line:
All Airflow units.

Environment:
All Serial Numbers

Cause:
Install/Repair

Resolution:

The below  schematic works for M400 & M800 actuators.  The system needs a 30VA transformer for the new actuator.  The actuator dipswitches need to be adjusted for Floating [24v open & 24v close] dipswitches 1 & 2 on and the rest off.

Manual Operation
There is a red manual operation handle on the actuator, see figure 2.  When it is lowered, the motor stops. Then the actuator can be operated manually if the handle is turned.

Original Wiring

Original Wiring

New Wiring

New wiring

ATTENTION: Actuators are shipped with manual override lowered (MAN). For normal operating, the handle must be raised (AUTO).
Actuator

Schneider Electric Algeria

Pièce(s) jointe(s)
DG5 to m400-m800 Actuator rev. 20111220.pdf [28.09 KB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :