{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Will the NetShelter CX fit through standard doors?
Issue:
Will the CX fit through a standard door opening?

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Need to ensure the NetShelter CX will fit up the stairs, into the elevator or through a doorway.

Resolution:
All the units, including the 38U, are designed to go through a standard doorway. They measure 750 mm /29.5” wide x max 1950mm/76.7” tall.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :