{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
Issue:
From what materials is the NetShelter CX is constructed?

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Environmental

Resolution:
The NetShelter CX is constructed using Melamine Faced Chipboard (MFC).

The NetShelter CX also uses a combination of Medium Density Fibre Board (MDF) and High Pressure Laminate (HPL) on its top and MDF on its plinth base.

The four acoustic foams & barriers which line the interior of the CX are:

Foam 1. Meets HF1 the highest rating for cellular foam products.

Foam 2. FT70 - flame retardant, compliant to BS476 part 6 ; class O, and cellular part 7: class 1, UL94-HF1 and UL94-VO and F.M.V.S.S 302

Foam 3. FT80 - flame retardant, compliant to BS476 part 7: class 1, UL94-HF1 and UL94-VO and F.M.V.S.S 302

Rubber.   CB-V0-02

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :