{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Does the ACSC automatically restart after a high head pressure alarm?
Issue:
Does the ACSC automatically restart after a high head pressure alarm?

Product line:
ACSC100, ACSC101

Environment:
InRow Cooling

Cause:

Resolution:
Yes, if the ACSC sees the HP switch open, it will switch into idle mode and then attempt to restart after a 2 minute delay. If the unit had the HP switch open three times within 30 minutes, the ACSC will go into Persistent High Discharge alarm and will lock out the compressor. This alarm will need to be reset manually.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :