{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What are the differences between APC branded and Dell branded Smart-UPS products?
Issue:

What are the differences between APC branded and Dell branded Smart-UPS?

Product Line:

Smart-UPS

Environment:

"DL" models,  All Serial Numbers

Cause:

APC has entered into an agreement with Dell to produce new Dell branded Smart-UPS. All support is to be provided by APC.

Resolution:

There are 5 differences between new Dell branded units and APC standard models:

1. Dell logo badge on the front panel.

2. Dell logo on the box.

3. Online Smart-UPS models (DLRTs) ship as towers, with feet and top cover attached, but include the rail kit in the box for versatility.
APC standard Smart-UPS Online products come either as a tower (no rail kit) or as a rackmount (no feet). DLRTs are true convertibles.

4.  Dell SKUs have a blue sticker on their rear panels:
Dell Label

5. All Dell branded units feature a 3 year Hardware and 3 year Battery warranty

APC provides all post-sales support for these products.  Customers should call APC directly rather than contacting Dell tech support.

Technical specs are the same between the APC and Dell branded units, with the exception of the DLRT8KRMXLT which features a 6 x L30-30 PDU instead of the 4 x L6-20 and 2 x L6-30 on the standard APC branded unit.
Dell-branded SKUDescription / Model NameAPC-branded SKU
DLRT192RMBPDell Smart-UPS SRT 192V 5kVA Tower/RM Battery PackSRT192RMBP
DLRT192RMBP2Dell Smart-UPS SRT 192V 8kVA Tower/RM Battery PackSRT192RMBP2
DLRT192RMBPJDell Smart-UPS SRT 192V Extended Battery Module for 5kVA UPS JapanSRT192RMBPJ
DLRT192RMXLBP3UDell Smart-UPS RT 192V RM Extended Battery ModuleSURT192RMXLBP3U
DLRT192RMXLBPJ3UDell Smart-UPS RT 192V RM Extended Battery Module for JapanSURT192RMXLBPJ3U
DLRT3000RMXLADell Smart-UPS SRT 3000VA RM 120V SRT3000RMXLA
DLRT3000RMXLIDell Smart-UPS SRT 3000VA RM 230V SRT3000RMXLI
DLRT5000RMXLJ3UDell Smart-UPS RT 5000VA RM 200VSURT5000RMXLJ3U
DLRT5KRMXLIDell Smart-UPS SRT 5000VA Tower/RM 230VSRT5KRMXLI
DLRT5KRMXLJDell Smart-UPS SRT 5kVA 200V JapanSRT5KRMXLJ
DLRT5KRMXLTDell Smart-UPS SRT 5000VA Tower/RM 208VSRT5KRMXLT
DLRT8000RMXLI6UDell Smart-UPS RT 8000VA RM 230VSURT8000RMXLI6U
DLRT8000RMXLT6UDell Smart-UPS RT 8000VA RM 208VSURT8000RMXLT6U
DLRT8KRMXLIDell Smart-UPS SRT 8000VA Tower/RM 230VSRT8KRMXLI
DLRT8KRMXLTDell Smart-UPS SRT 8000VA Tower/RM 208VSRT8KRMXLT
DLRT96RMBPDell Smart-UPS SRT 96V 3kVA Battery PackSRT96RMBP
DLRTA3000RMXL3UDell Smart-UPS RT 3000VA RM 120VSURTA3000RMXL3U
DLRTD3000RMXLI3UDell Smart-UPS RT 3000VA RM 230VSURTD3000RMXLI3U
DLRTD5000RMXLI3UDell Smart-UPS RT 5000VA RM 230VSURTD5000RMXLI3U
DLRTD5000RMXLT3UDell Smart-UPS RT 5000VA RM 208VSURTD5000RMXLT3U
DLT1200RMJ1UDell Smart-UPS 1200VA LCD RM 1U 100VSMT1200RMJ1U
DLT1500, DLT1500CDell Smart-UPS 1500VA LCD 120VSMT1500, SMT1500C
DLT1500IDell Smart-UPS 1500VA LCD 230VSMT1500I
DLT1500JDell Smart-UPS 1500VA LCD 100VSMT1500J
DLT1500RM2UDell Smart-UPS 1500VA LCD RM 2U 120VSMT1500RM2U
DLT1500RMI2UDell Smart-UPS 1500VA LCD RM 2U 230VSMT1500RMI2U
DLT1500RMJ2UDell Smart-UPS 1500VA LCD RM 2U 100VSMT1500RMJ2U
DLT2200Dell Smart-UPS 2200VA LCD 120VSMT2200
DLT2200IDell Smart-UPS 2200VA LCD 230VSMT2200I
DLT3000RM2UDell Smart-UPS 3000VA LCD RM 2U 120VSMT3000RM2U
DLT3000RMI2UDell Smart-UPS 3000VA LCD RM 2U 230VSMT3000RMI2U
DLT3000RMJ2UDell Smart-UPS 3000VA LCD RM 2U 100VSMT3000RMJ2U
DLT750JDell Smart-UPS 750VA LCD 100VSMT750J
DLX120RMBPJ2UDell Smart-UPS X 120V External Battery Pack Rack/Tower for JapanSMX120RMBPJ2U
DLX3000RMLVJ2UDell Smart-UPS X 3000 Rack/Tower 100VSMX3000RMLVJ2U


Please see attached sales brochures for images and additional information.

Schneider Electric Algeria

Pièce(s) jointe(s)
DELL 230V Brochure.pdf [1.98 MB]
DELL NAM Brochure .pdf [4.48 MB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :