{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Does the NetShelter CX interfere with a device's wifi signal? If it does, by what degree is the signal strength reduced?

Issue:
Need to determine if the NetShelter CX can effect wifi signal strength.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Wireless devices can be installed inside a NetShelter CX cabinet.

Resolution:
A wireless device was tested in the NetShelter CX manufacturing facility. The signal strength was affected by less than 10% in 3 of the test areas and by 38.46% in 1 of the areas. The test results show that the Office had the greatest signal reduction but only dropped to a Fair signal strength. None of the results indicated a poor or unusable signal.

A complete test report is attached below.

Schneider Electric Algeria

Pièce(s) jointe(s)
20140324 WIFI TEST RESULTS.pdf [187.42 KB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :