{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Is there a document available that shows which roof height adapters are used in various applications like EcoAisle and InRow?

Issue:
There's a need to confirm the correct roof height adapter; that it's compatible with the product and application where it's being installed.

Product Line:
InRow Cooling, NetShelter SX, NetShelter VX

Environment:
All versions and serial ranges.

Cause:
There are a few PDUs which don't have mounting holes for roof height adapters, and there is need to help choose the correct roof height adapter for a particular application.

Resolution:
See attached file

Schneider Electric Algeria

Pièce(s) jointe(s)
20140429 Roof Height Adapter Compatibility Chart Rev 3.pdf [208.2 KB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :