{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Is there a roof fan available for the NetShelter SV cabinets?

Issue:
There does not appear to be an optional roof fan for the NetShelter SV cabinets.

Product Line:
NetShelter SV

Environment:
All versions and serial ranges.

Cause:
A request has been made to add a roof fan to a NetShelter SV.

Resolution:
The NetShelter SV cabinets do not currently have roof fans available.
Some of the fans that can be used inside the SV cabinet are: ACF001, ACF002, ACF003, ACAC40001, ACF201BLK, ACF202BLK.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :