{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
APC UPS Network Management Card (NMC) Compatibility Chart

Article available in these languages: Espagnol

Issue

Which model of UPS Network Management Card is supported in my UPS?


Product Line

  • UPS Network Management Card for Easy UPS Online - AP9544
  • UPS Network Management Card for Easy UPS, 3-Phase - AP9547
  • UPS Network Management Card 3 - AP9640, AP9641, AP9643
  • UPS Network Management Card 4 - AP9644
  • UPS Network Management Card 2 - AP9630/30CH, AP9631/31CH, AP9635/35CH
  • UPS Network Management Card 1 - AP9617, AP9618, AP9619
  • UPS Web/SNMP Card - AP9606

Environment

  • All firmware versions (unless otherwise specified)
  • All serial numbers


Cause

This compatibility chart has been created for reference.


Resolution

Please refer to the table below.

Note: Some of these management cards are older and discontinued. This means while there may be some compatibility between current UPS models and discontinued management cards, support for new device features or management card features and bug fixes will only be available with the current generation of Network Management Card for your device. Current generation Network Management Cards purchased on their own will ship with the SUMX application file, for use with the Smart-UPS family. Firmware files for use in other UPS systems can be found here: http://www.apc.com/us/en/tools/download/ (Filter by Software/Firmware and choose "Firmware Upgrade")

Network Management Card Model(s)UPS ModelNote(s)
AP9547
  • All Easy UPS 3S 10-40 kVA UPS models
  • All Easy UPS 3M 60-200 kVA UPS models
  • All Easy UPS 3L 250-600 kVA UPS models
  • All Galaxy 3L 250-600 kVA UPS models
  • All Galaxy PW 2nd Gen. 10-200 kVA UPS models
AP9547 does not support Easy UPS 3-Phase  Modular.
AP9544
  • Single-phase Easy UPS On-Line with the following prefixes and kVA:
    • SRV 1-3 kVA, SRVL 1-3 kVA
    • SRV 5-20 kVA
  • Single-phase Easy UPS 1 Ph On-Line with the following prefixes and kVA:
    • SRVS 1-3 kVA, SRVSL 1-3 kVA
    • SRVS 5-10 kVA
An alternate bracket is included in the box with the NMC card and must be screwed to the NMC before it can be inserted into the UPS device’s SmartSlot. This is applicable to below UPS models only:
o            SRV1KA
o            SRV1KA-TW
o            SRVPM6KRI
o            SRVPM6KRI-TW
o            SRVPM6KRIL
o            SRVPM6KRIL-TW
o            SRVSPM6KRI
o            SRV15KUXI-IN
o            SRV20KUXI-IN
o            SRVPM6KRILPK
o            SRV1KA-CA
o            SRV5KL-IN
o            SRV6KL-IN
o            SRV5KUXI-IN
o            SRV6KUXI-IN
o            SRV10KUXI-IN
o            SRVPM5KRI
o            SRVSPM5KRI
o            SRVSPM5KRIL
o            SRVPM10KRIL-IN
o            SRVPM10KRI
o            SRVSPM10KRI
AP9640, AP9641, AP9643
  • Single and Three Phase Smart-UPS with the following model prefixes:
    • SUA*
    • SUM
    • SURT
    • SURTA
    • SURTD
    • SUVT & MGE Galaxy 3500
    • SMT
    • SMX
    • SRT
    • SRC
    • SMTL
    • SRTL
    • SRYL
    • Symmetra LX (Single phase Symmetra UPS)
    • Symmetra RM (v1.5.1.1 and greater)
  • Three phase models:
    • Symmetra PX1 (20kW, 40kW, 48kW)
    • Symmetra PX2 (96kW, 100kW, 160kW)
    • Symmetra PX 250/500 (250kW, 500kW) - AP9643 only
    • Galaxy VM
    • Galaxy VX
    • Galaxy PX - AP9640/AP9641 only
    • Easy UPS 3-Phase Modular - AP9640/AP9641 only
    • Easy UPS 3M Advanced - AP9640/AP9641 only
  • *Note: SUA devices manufactured after 2008, with firmware version v1.4.2 and above.
  • *Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution.
AP9644
  • Three Phase Galaxy UPS units:
    • Galaxy VS
    • Galaxy VL
    • Galaxy VXL


Notes:
  1. The listed units include a built-in network management card
  2. The AP9644 card is supported on the Galaxy VS from UPS firmware revision v6.31.3.x.
    • The AP9644 card is backward compatible with any Galaxy VS already installed. When the card is installed after the UPS, however, a new Start-up service (WSTRTUP-VS1-A50) needs to be purchased to upgrade the UPS and the card at the site.
AP9630/30CH, AP9631/31CH
  • Single and Three Phase Smart-UPS with the following model prefixes:
    • SU
    • SUA
    • SUM
    • SURT
    • SURTA
    • SURTD
    • SUVT & MGE Galaxy 3500
    • SMT
    • SMX
    • SRT
    • SRC
  • Matrix UPS with UPS firmware versions Y or Z
    • MX3000
    • MX5000
  • Single phase Symmetra models:
    • Symmetra Power Array
    • Symmetra RM
    • Symmetra LX
  • Three phase Symmetra models:
    • 48kW Symmetra PX2 All-In-One*
    • 20kW Symmetra PX
    • 40kW Symmetra PX
    • 80kW Symmetra PX
    • 100kW Symmetra PX2*
    • 160kW Symmetra PX2*
  • SMX/SMT require sumx APP v5.0.3 or higher.
  • SRT models require sumx APP v6.0.7, or v6.2.0 or higher
  • *Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution.
AP9630/30CH, AP9631/31CH, AP9635/35CH
  • Three Phase Galaxy UPS units
    • ​Galaxy 300/7000*
    • Galaxy VM
  • *Ships with AP9630 pre-installed in units manufactured post 2012. Older G7000 models require a special upgrade kit pre-2012 manufacture date.
AP9635/35CH
  • 3 Phase UPS models including:
    • Symmetra PX 250/500
    • SUVT/G500*
    • Symmetra PX 20/40/80
    • Symmetra PX2 48kW All-in-One*
    • Symmetra PX2 100/160 kW*
  • Single Phase UPS models including:
    • Smart-UPS*
    • Symmetra*
  • *With AOS 6.4+ only, modem features only supported on MGE Galaxy units
  • **When using a NMC with an embedded NMC/Brain the FW file revisions must match. IE. 6.50 with 6.50, 6.8 with, 6.8, etc. Failure in doing so will cause communication alarms and display malfunction.
G5K9635CH
  • MGE Galaxy 5000
  • Kit includes all necessary parts to install an AP9635 for all G5000 UPS serial numbers and firmware.
G9K9635CH
  • MGE Galaxy 9000
  • Kit includes all necessary parts to install an AP9635 for all G9000 UPS serial numbers and firmware.
AP9617, AP9618, AP9619
  • Single and Three Phase Smart-UPS with the following model prefixes:
    • SU
    • SUA
    • SUM
    • SURT
    • SURTA
    • SURTD
    • SUVT*
  • Matrix UPS with UPS firmware versions Y or Z
    • MX3000
    • MX5000
  • Single phase Symmetra models:
    • Symmetra Power Array
    • Symmetra RM 6K/12K
    • Symmetra LX
  • Three phase Symmetra models:
    • 20kW Symmetra PX All-In-One
    • 40kW Symmetra PX
    • 80kW Symmetra PX
    • 100kW Symmetra PX2**
    • 160kW Symmetra PX2**
  • Silcon
  • *Note: SUVT model UPSs with v7.X.X firmware should use NMC2 to take advantage of all UPS firmware enhancements.

**Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution.
AP9606
  • Older UPS models including:
    • Smart-UPS with the following model prefix:
      • SU
      • SUA
    • Symmetra Power Array
    • Symmetra RM 6K/12K
    • Matrix UPS with UPS firmwares Y or Z
      • MX3000
      • MX5000
    • 40kW Symmetra PX
    • 80kW Symmetra PX
  • Silcon
  • 0J-0N-9581GVM
  • Galaxy VM
  • Spare part for Galaxy VM Display/Embedded Network Management Card inside
0G-9354
W0G-9354 (spare part)
0G-9354A
0J-0G-9354A (spare part)
  • Three phase Symmetra (PX2) models:
    • 48kW Symmetra PX All-In-One
    • 100kW Symmetra PX
    • 160kW Symmetra PX
  • UPS brain with embedded Network Management Card.
  • "A" SKU's are built on NMC2 architecture


Note: Certain features are limited by application.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :