{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
How tall is the NetShelter WX with the optional castor kit attached?
Issue:
Customers may ask for the total height of the NetShelter WX with the optional castor kit attached.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
Cabinets that are floor mounted may have height restrictions.

Resolution:
The NetShelter WX with the optional castor kit attached is approximately 731 mm (28.78") tall.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :