{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What is the cfm rating of the NetShelter CX with AR4703 installed?
Issue:
Customers want to know the cfm rating of NetShelter CX cabinets with the AR4703 fan booster installed.

Product Line:
NetShelter CX.

Environment:
All versions and serial ranges.

Cause:
Installing the AR4703 increases the cfm of the NetShelter CX cabinet.

Resolution:
18U  with 1x AR4703 - 260 CFM
24U  with 2x AR4703 - 330 CFM
38U  with 3x AR4703 - 340 CFM

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :