{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.

Consulter notre FAQ

Can the Combination Lock Handle or PX-HID Lock be installed onto the ARU?

Issue:
Customer requests compatibility information between the Combination door handle or PX-HID lock, and the ARU.

Product Line:
NetShelter SX ARU, NetBotz PX-HID

Environment:
All versions and serial ranges.

Cause:
Customer requires secure access to the ARU.

Resolution:
The Combination Lock Handle and PX-HID Lock are not compatible with the ARU.
If additional security is required, the lock cylinder can be replaced to accept a unique key, as described in FAQ FA158606: http://www.apc.com/us/en/faqs/FA158606/

Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :