{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)

Issue

Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2).


Product Line
  • UPS Network Management Card 2 - AP9635/AP9635CH


Environment
  • Data centers with products that use AP9635/AP9635CH Network Management Card 2 (NMC2)
  • Firmware applications that support Modbus TCP or Modbus RTU with AP9635/AP9635CH (Galaxy VM, Galaxy 300/7000, Galaxy 5000/5500, etc)


Cause

This application note explains how to install the Modbus wiring for an AP9635/AP9635CH Network Management Card 2, gives an overview of the Modbus protocol, describes the Modbus packet structure, and explains how to identify and resolve common problems.

(​The Modbus protocol uses TCP, RTU and ASCII modes of transmission. The AP9635/AP9635CH supports Modbus/TCP and Modbus/RTU protocols.)


Resolution
The latest version of the Modbus Installation and Troubleshooting for AP9635/AP9635CH Management Card Application Note 168 attached below.

Schneider Electric Algeria

Pièce(s) jointe(s)
AKAR-8KETBK_R3_EN.pdf [710.43 KB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :