{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Using AP9613 simultaneously in the same UPS system as a UPS Network Management Card causes lost communication alarms

Issue

Using AP9613 Dry Contacts I/O SmartSlot Card simultaneously in the same UPS system as a UPS Network Management Card causes lost communication alarms within the UPS Network Management Card event log.



Product Line
  • UPS Management Accessories
    • AP9613 Dry Contacts SmartSlot I/O Card
  • UPS Network Management Card 2 (NMC2)
    • AP9630/AP9630CH
    • AP9631/AP9631CH
    • AP9635/35CH

Environment
  • All serial numbers
  • All firmware versions
  • Older UPS designs (including but not limited to Smart-UPS with model SU, SUA, SUM, SURT, SURTA, Symmetra PX 3 phase 40/80, Symmetra LX, Symmetra RM)
  • UPS installations with both AP9613 and a UPS Network Management Card communicating with the same UPS


Cause

Due to the way older UPS serial bus designs operate, the AP9613 may prevent a UPS Network Management Card from communicating with the UPS, assuming they are both installed in the same UPS.


Resolution

This is a race condition. AP9613 firmware v2.1.0 has partially addressed this timing problem and a future firmware update for UPS Network Management Card 2 will be evaluated. Until a full fix is implemented, a user may see a UPS: Lost the local network management interface-to-UPS communication. periodically in their UPS Network Management Card log when the AP9613 is also installed. With AP9613 v2.1.0 and higher, this alarm should not remain permanently.

Schneider Electric Algeria