{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What size wrench is needed to remove the NetShelter pallet bracket?
Issue:
Customer may ask what size the pallet bracket bolts are.

Product Line:
NetShelter SX, NetShelter SV, NetShelter VX

Environment:
All versions and serial ranges.

Cause:
Customer wants to make sure they have the proper tools on hand.

Resolution:
NetShelter SX, SV and VX pallet brackets require a 13 mm wrench.
The NetShelter SV also requires a T30 Torx wrench (included). If the bolts are too tight for the included T30 Torx tool please use a T30 Torx socket and socket wrench.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :