Issue:
Questioning if there is a reason they should not plug an ARU into the PDU.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Not sure if an ARU can be plugged into a PDU.
Resolution:
It is perfectly fine to plug an ARU into a PDU.
Questioning if there is a reason they should not plug an ARU into the PDU.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Not sure if an ARU can be plugged into a PDU.
Resolution:
It is perfectly fine to plug an ARU into a PDU.
Publié pour:Schneider Electric Algeria