{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
How do I upgrade the PowerChute Network Shutdown (PCNS) application running on the Virtual Appliance.
Issue:
It's crucial to upgrade the version of PowerChute Network Shutdown installed on the PowerChute virtual appliance. This will ensure you have the latest features and security updates.

Product Line:
PowerChute Network Shutdown

Environment:
PowerChute Network Shutdown VM

Cause:
A newer version of PowerChute Network Shutdown is available.

Solution:

To run an updated version of PowerChute, power off the current PowerChute VM and install the latest version of the PowerChute Virtual Appliance. The latest version will contain updated security and an updated version of Linux. We do not support upgrading the version of PowerChute running on the PowerChute VM.

NOTE: If your PowerChute VM has an assigned license, the license must be released/returned before powering off the VM and installing the new VM. See Schneider Electric FAQ000259017 How to reuse-return a PowerChute Network Shutdown license?

Before installing the new Virtual Appliance, it is important to save the PowerChute configuration from the older version. To do this, log in to the current PowerChute Virtual Appliance and navigate to /opt/APC/PowerChute/group1. From there, save a copy of the pcnsconfig.ini file. Once the new Virtual Appliance is installed, you can transfer the saved pcnsconfig.ini file to the new Virtual Appliance. This will ensure that PowerChute uses the same configuration as before.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :