{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.

Consulter notre FAQ

Video: Data Center Expert | How do I use search filters?

Issue:
How to use search filters within StruxureWare Data Center Expert.

Product Line:
StruxureWare Data Center Expert (DCE)

Environment:
StruxureWare Data Center Expert (all versions)

Cause:
As the StruxureWare Data Center Expert deployment matures over time the number of device and sensor will increase as well. Which can make search for a given device or sensor increasingly difficult.

Resolution:
StruxureWare Data Center Expert has search filters that can be used to narrow a search down as small as possible. The article provides and explains each search option to assist with that search.



This filter option are executed but entering the command in upper case letting. All search functions will search multiple columns and are not isolated to one search field.

AND

The first would be the AND search function. This search function allows for a two or more word search if they are not consecutive.

OR

The second would be the OR search function. This search function allows for either keyword to be searched.

NOT

The last search function would be NOT. Using this function to be used to exclude keywords from the search.

To narrow the search as much as possible search function can be used in combination.

Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :