{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
What HID cards are supported by NetBotz rack access AP9361, NBPD0170 pod, and NetBotz 250/750/755.

Issue:
HID cards supported by NetBotz rack access AP9361 and NBPD0170 pod

Product Line:
NetBotz

Environment:

NetBotz Rack Access AP9361 units
NBPD0170 pods,
NetBotz 250 with Rack Access

Cause:
The current hardware and firmware supports specific HID cards

Resolution:

Please note that this information is in the manuals for these devices as well and the card listings may be updated without notice in this k-base.

The Rack Access PX-HID and NetBotz NBPD0170 pod supports four access card formats. The available formats are:
• H10301—Standard 26 bit: An access card with a 26-bit card ID number and a facility code.
• H10302—37 bit w/o facility code: An access card with a 37-bit card ID number and no facility code.
• H10304—37 bit w/ facility code: An access card with a 37-bit card ID number and a facility code.
• Corporate 1000: An access card with a 35-bit card ID number and a unique company ID code.

The Rack Monitor 250/750/755 with the NetBotz 125 kHz Handle Kit (NBHN0125) supports the following 125kHz
proximity cards:
• H10301 26-bit
• H10302 - 37 bit
• H10304 - 37bit with facility code
• CORP-1000

The Rack Monitor 250/750/755 with the NetBotz 13.56 MHz Handle Kit (NBHN1356) supports the following
13.56MHz proximity cards:
• MIFARE Classic 4-byte UID
• MIFARE Classic 7-byte UID
• MIFARE DESFIRE
• MIFARE PLUS

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :