{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Can a 63.75" tall PDU be installed into a 38U NetShelter CX cabinet?
Issue:
The 63.75" tall PDU does not fit onto the accessory rail. Will it fit anywhere else inside the cabinet?

Product Line:
NetShelter CX

Environment:
AR4038A, AR4038IA

Cause:
One of the 63.75" tall PDUs has been specc'd into a 38U NetShelter CX cabinet.

Resolution:
Yes, the 63.75" tall PDUs can attach to the rear mounting rail. Please see the attached file for mounting instructions.

Schneider Electric Algeria

Pièce(s) jointe(s)
20160729 Tall PDU Mounting Into 38U NetShelter CX.docx [5.95 MB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :