Consulter notre FAQ
The PowerChute Network Shutdown Windows Installer is susceptible to a DLL hijacking vulnerability
Issue:
The PowerChute Network Shutdown Windows Installer is susceptible to a DLL hijacking vulnerability
Product:
PowerChute Network Shutdown v4.1 and earlier
Environment:
Microsoft Windows operating systems
Cause:
The PowerChute Network Shutdown Windows installer is created using Nullsoft Scriptable Install System (NSIS). Certain versions of NSIS are vulnerable to DLL hijacking (also known as DLL preloading). DLL Hijacking occurs when a malicious DLL is downloaded to the same directory from which the vulnerable NSIS installer will run (e.g. a default web downloads directory). The malicious DLL can then be loaded and executed, potentially with escalated privileges.
See Microsoft Security Advisory 2269637 for more information on the vulnerability.
Solution:
This issue has been fixed in the Windows installer for PowerChute Network Shutdown v4.2 and above.
For v4.1 and earlier, please refer to the Suggested Actions section of the Microsoft Security Advisory 2269637
The PowerChute Network Shutdown Windows Installer is susceptible to a DLL hijacking vulnerability
Product:
PowerChute Network Shutdown v4.1 and earlier
Environment:
Microsoft Windows operating systems
Cause:
The PowerChute Network Shutdown Windows installer is created using Nullsoft Scriptable Install System (NSIS). Certain versions of NSIS are vulnerable to DLL hijacking (also known as DLL preloading). DLL Hijacking occurs when a malicious DLL is downloaded to the same directory from which the vulnerable NSIS installer will run (e.g. a default web downloads directory). The malicious DLL can then be loaded and executed, potentially with escalated privileges.
See Microsoft Security Advisory 2269637 for more information on the vulnerability.
Solution:
This issue has been fixed in the Windows installer for PowerChute Network Shutdown v4.2 and above.
For v4.1 and earlier, please refer to the Suggested Actions section of the Microsoft Security Advisory 2269637
Publié pour:Schneider Electric Algeria
En savoir plus
Gamme :
Catégorie :
En savoir plus
Gamme :
Catégorie :