{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Proper use of a "Make Before Break" bypass panel with an SURT or SRT UPS
Failure to follow the below instructions may result in the following fault messages on the SmartUPS:
P.11, SRT DC Bus Overvoltage, Event 118, Event 119, failure bypass

IMG1 IMG1 IMG1 IMG1

When moving from Normal to Test mode:

●Place UPS into internal Bypass
●Confirm UPS is in Bypass
●It is now safe to move the SBP to Test mode

When moving from Test to Bypass or vice versa:
●UPS can be in any state

When moving from Test back to Normal:

Place UPS into internal Bypass
●Confirm that UPS is in Bypass
●Move SBP to Normal
●Confirm UPS has no faults and input is acceptable to bring online.
●Take UPS out of internal Bypass

Schneider Electric Algeria

En savoir plus
Produit :
Gamme :
En savoir plus
Produit :
Gamme :