{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Unable to open the AP9613 - dry contact I/O card configuration utility in Windows 10
Issue

Users are unable to open the AP9613 dry contact I/O card configuration utility in Windows 10. When connecting the card to the PC/laptop for the first time the following error messages are displayed when attempting to open the card's removable drive in Windows File Explorer:

Win 10 Fault

Win 10 fault 2

On subsequent connections to the same PC/laptop these error messages are not displayed; the card's removable drive is also not displayed.

Win 10 Fault 3

Product Line

AP9613 - Dry Contact I/O SmartSlot Card.

Environment
  • AP9613 - all serial numbers. Firmware revision 210.
  • Operating System:  Microsoft Windows 10, version 10.0.14393, build 14393.

Cause

Users are unable to open the dry contact I/O card configuration utility when the AP9613 is connected with the supplied USB cable to a PC/laptop running Windows 10 (version 10.0.14393, build 14393). Testing performed on this issue shows that PC/laptops running OS versions prior to and after the 10.0.14393 version (build 14393) do not exhibit this issue.

Resolution

Update the operating system to the latest stable version.

Schneider Electric Algeria

En savoir plus
Produit :
Les articles qui pourraient être utiles
En savoir plus
Produit :