{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Are there instructions showing the proper way to install the gasket material of a Vertical Exhaust Duct Kit?
Issue:
Pieces of the gaskets are loose or falling off.

Product Line:
Vertical Exhaust Duct Kits

Environment:
All versions and serial ranges

Cause:
If the gasket is not installed properly it will not adhere.

Resolution:
The installation manual has been updated with instructions for correctly installing gaskets to the top of the duct, and NetShelter door frame.
You can also find a gasket installation video from Trim-Lok at this link: https://www.trimlok.com/rsinstall
There is also a document attached below that explains correct installation of the gasket.

Spare Gaskets:
We may have 8.4m pieces of the gasket used on the door frame in stock as spare part 0J-827-0292A.
We do not have spares for the gasket used atop the duct. It's Trim-Lok pn: X-1153HT-SINGLE. (HT, Black, single) Trim-Lok sells this by the 1,000 foot box.
https://www.trimlok.com/rubber-extrusion/epdm-seal/d-profile/1153-series

Schneider Electric Algeria

Pièce(s) jointe(s)
20170425 VED Kit Gasket Installation Instructions rev1.pdf [31.79 KB]
En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :