Consulter notre FAQ
Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL
Issue:
Where to find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL
Product line:
SYBTU1-PLP / SYBTU2-PLP, GVSBTU/GVSBTHU/GVSBTHULL
Environment:
PX1,2, 250-500, SUVT, Galaxy 3500, Galaxy VS
Information:
See application note 143 for specific values of contained electrolyte in both the SYBTU1-PLP (used in PX1 20,40, 48, 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units) and the SYBTU2-PLP (used in the PX2 100KVA and the PX 250/500KVA UPS units) batteries.
Application Note 143:
http://www.apc.com/salestools/SMCR-6NXGXU/SMCR-6NXGXU_R2_EN.pdf
Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. For further information on MSDS by the specific vendors please refer to FA157067
Also see FA157067
Galaxy VS Modular Batteries:
Where to find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL
Product line:
SYBTU1-PLP / SYBTU2-PLP, GVSBTU/GVSBTHU/GVSBTHULL
Environment:
PX1,2, 250-500, SUVT, Galaxy 3500, Galaxy VS
Information:
See application note 143 for specific values of contained electrolyte in both the SYBTU1-PLP (used in PX1 20,40, 48, 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units) and the SYBTU2-PLP (used in the PX2 100KVA and the PX 250/500KVA UPS units) batteries.
Application Note 143:
http://www.apc.com/salestools/SMCR-6NXGXU/SMCR-6NXGXU_R2_EN.pdf
Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. For further information on MSDS by the specific vendors please refer to FA157067
Also see FA157067
Galaxy VS Modular Batteries:
Battery Type | Electrolyte Weight | Electrolyte Volume | ||
(kg) | (lbs) | (ml) | (gal) | |
GP1272F2FR | 0.5 | 1.11 | 378 | 0.1 |
HR1234WF2FR | 0.44 | 0.98 | 333 | 0.09 |
UP-PW1245P1 | 0.4794 | 1.057 | 378 | 0.0998 |
Battery Type | Electrolyte Weight | Electrolyte Volume | ||
(kg) | (lbs) | (ml) | (gal) | |
GVSBTU | 5 | 11.1 | 3780 | 1 |
GVSBTHU | 4.4 | 9.8 | 3330 | 0.9 |
GVSBTHULL | 4.794 | 10.57 | 3780 | 0.998 |
Battery Type | Electrolyte Weight | Electrolyte Volume | ||
(kg) | (lbs) | (ml) | (gal) | |
GVSBT4 | 20 | 44.4 | 15120 | 4 |
GVSBTH4 | 17.6 | 39.2 | 13320 | 3.6 |
GVSBTH4LL | 19.176 | 42.28 | 15120 | 3.992 |
Publié pour:Schneider Electric Algeria
Pièce(s) jointe(s)
En savoir plus
Gamme :
En savoir plus
Gamme :