{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
PowerChute Network Shutdown shuts down an ESXi host in vSAN cluster before it has been moved to maintenance mode.
Issue:
PowerChute Network Shutdown shuts down an ESXi host in vSAN cluster before it has been moved to maintenance mode.

Product Line:
PowerChute Network Shutdown (PCNS) version 4.2

Environment:
  • vSAN cluster containing 3 x VMware ESXi 6.5 Hosts (H1, H2, H3)
  • All servers are protected by 1 UPS
  • PowerChute and vCenter Server are installed on a physical server outside the HA cluster
  • Data is located on ESXi Hosts H1 & H2, H3 is a witness server, VM setting is "FTT = 1"
Symptoms:
  • PowerChute starts a shutdown sequence and the hosts set to move to maintenance mode
  • ESXi hosts H1 and H3 move to maintenance mode as expected
  • ESXi host H2 does not move to maintenance mode
Note: The following message appears in the Event Log indicating that a host has failed to enter maintenance mode:

Failed to enter maintenance mode on Host <H2>
  • ESXi hosts H1, H2 & H3 are shut down.
Cause:
There is a known VMware issue whereby the last host is unable to move to maintenance mode.

Resolution:
Upgrade to PowerChute Network Shutdown 4.3

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :