{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Which External Battery Pack (XLBP) and RBC is compatible with my Smart-UPS On-Line (SRT) model?

Article available in these languages: Espagnol, Thaï


Issue:

Which External Battery Pack (XLBP) and RBC is compatible with my Smart-UPS On-Line (SRT) model?

Product Line:

Smart-UPS Online

Environment:

All SRT models and all SRT external battery packs, All Serial Numbers

Cause:

There are specific External Battery Pack and RBC models which are compatible with a group of UPS models.

Resolution:

When selecting an External Battery Pack (XLBP) or RBC for a UPS system, use the table below to select compatible models.

NOTE: Each external battery pack has a keyed mating connector that is only compatible with its corresponding UPS. If you find that a connector is binding or requires excessive force to insert you should STOP and check compatibility of the UPS and battery pack.
UPS Model (beginning with)Battery TypeReplacement Battery Pack (RBC)Battery Module VoltageTotal Battery Voltage for the UPSExternal Battery Pack Connector ColorExternal Battery Pack (XLBP)
SRT1000XL, SRT1500XL, SRT1000RMXL, SRT1500RMXLMaintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproofAPCRBC15548 VDC48 VDCBlueSRT48BP
SRT48RMBP
SRT1000UXI-LI, SRT1500UXI-LILithium Ion NMC chemistryNo internal battery - uses external battery systemNASee manualBlueXBP48RM1U-LI
Note: The UPS does not
support any other make/type of battery packs.
SRT2200XL, SRT2200RMXLMaintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproofAPCRBC14172 VDC72 VDCGreenSRT72BP
SRT72RMBP
SRT3000XL, SRT3000RMXLMaintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproofAPCRBC15296 VDC96 VDCBrownSRT96BP
SRT96RMBP
SRT5K, SRT6KMaintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproofAPCRBC14096 VDC192 VDCWhiteSRT192BP
SRT192RMBP
SRT8K, SRT10KMaintenance-free sealed Lead-Acid battery with suspended electrolyte : leakproofAPCRBC14096 VDC+192 VDC
-192 VDC
WhiteSRT192BP2
SRT192RMBP2


Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :