Product Line
Symmetra LX
Symmetra RM
Symmetra Power Array
Resolution
When the EPO on the single phase Symmetras is triggered it will cause the System Enable switch (on/off switch) to physically move to the "off" position. Regardless of what state the UPS is in (On battery, On line, In Bypass) the Symmetra will immediately be powered off entirely. This includes all load attached.
Symmetra LX
Symmetra RM
Symmetra Power Array
Resolution
When the EPO on the single phase Symmetras is triggered it will cause the System Enable switch (on/off switch) to physically move to the "off" position. Regardless of what state the UPS is in (On battery, On line, In Bypass) the Symmetra will immediately be powered off entirely. This includes all load attached.
Publié pour:Schneider Electric Algeria