{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
SmartConnect Smart-UPS loses connectivity with the cloud after a period of time.

Article available in these languages: Allemand

Issue:
SmartConnect Smart-UPS loses connectivity with the cloud after a period of time.

The symptoms are
  • Status page in SmartConnect Portal shows "Communications Lost" for the device.
  • UPS LCD Display shows SmartConnect status as "SC.4" or "Contacting" depending on the device type.

Product Line:
SmartConnect Smart-UPS

Environment:
SmartConnect Smart-UPS

Cause:
Firmware

Solution:
Reboot the network interface of the Smart-UPS per the instructions in FAQ FA322105. Once communications has been re-established with the cloud verify the UPS firmware is up-to-date. To verify the firmware version log in to SmartConnect.apc.com. Go to Dashboard, select view UPS from the list of UPS, select Device to view the UPS firmware version.

Verify your firewall will allow connectivity to the cloud server. See Schneider Electric FAQ000230321 Network Requirements for APC SmartConnect portal.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :