Smart-UPS Lithium-Ion units will not perform a battery calibration
Product Line:
Smart-UPS
Environment:
SMTL750RM2UC, SMTL1000RM2UC, SMTL1500RM3UC - All Serial Numbers
Cause:
Smart-UPS Lithium-Ion units do not support battery calibration.
Resolution:
The Lithium-Ion Smart-UPS platform does not require runtime calibrations to provide accurate runtime estimates. The calibration option has been removed from the LCD interface of the UPS. If you are using the web interface of a Network Management Card you will still see the battery calibration option, however it will not initiate. This is normal behavior.
Publié pour: Schneider Electric Algeria
Smart-UPS Lithium-Ion units will not perform a battery calibration
Product Line:
Smart-UPS
Environment:
SMTL750RM2UC, SMTL1000RM2UC, SMTL1500RM3UC - All Serial Numbers
Cause:
Smart-UPS Lithium-Ion units do not support battery calibration.
Resolution:
The Lithium-Ion Smart-UPS platform does not require runtime calibrations to provide accurate runtime estimates. The calibration option has been removed from the LCD interface of the UPS. If you are using the web interface of a Network Management Card you will still see the battery calibration option, however it will not initiate. This is normal behavior.
Publié pour: Schneider Electric Algeria




Besoin d'aide ?
Commencez ici !
Trouvez des réponses dès à présent Rechercher une solution par vous-même ou contacter l'un de nos experts.
Contactez le support
Contactez notre équipe du service client pour obtenir plus d'informations, un support technique, une assistance en cas de plaintes, etc.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Parcourir la FAQ
Obtenez les réponses dont vous avez besoin en parcourant la foire aux questions (FAQ) par sujet.
Contacter le service commercial
Effectuez une demande de renseignements en ligne et un expert vous contactera.