{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.

Consulter notre FAQ

Galaxy VX; Customer, consultant or engineer looking for the center of gravity (CoG) for the IO and/or PC enclosures


Issue:
Customer, consultant or engineer looking for the Center of Gravity (CoG) for the IO and/or PC enclosures.


Product line:
Galaxy VX


Environment:
All models, all serial numbers


Cause:
none.


Resolution:
The enclosures have the following CoG.
  • GVX PC: X-distance 290mm, Y-distance 930mm , Z-distance 440mm
  • GVX 750kW IOC: X-distance 590mm, Y-distance 830mm, Z-distance 390mm
  • GVX 1000kW IOC: X-distance 590mm, Y-distance 830mm, Z-distance 390mm
  • GVX 1500kW IOC: X-distance 1060mm, Y-distance 970mm, Z-distance 430mm
  • GVXMBCR750: X-distance 399.7mm, Y-distance 993mm, Z-distance 471.5mm

(X=width, Y=height, Z=depth)



Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :